Part Number: DP83TG720EVM-MC
Hi I currently have a custom design on an FPGA board that uses the DP83TG720RWRHATQ1. The strapping resistors on the custom PCB have the DP83TG720RWRHATQ1 set to RGMII, autonomous and slave mode with RX and TX shift mode.
I am currently trying to connect the custom board to the DP83TG720EVM-MC that then connects to the computer to ping the FPGA and test our automotive ethernet design. After I connect the hardware and attempt to ping the static IP address on my FPGA through my PC - I am unable to reach it. I also notice that the link LED and activity LED do not blink and are off on the eval board.
Is there any further setup needed through MDIO to setup the DP83TG720RWRHATQ1 or are the strapping resistors enough? Thank you for any feedback and guidance in advance.