Other Parts Discussed in Thread: INA228, LSF0102-Q1, TCA9517, LSF0102
Hi experts,
We have an automotive application where the I2C master and RTC are running on 3.3V logic and an EEPROM, INA228AQDGSRQ1 and LCD interface are running on 5V logic. We considered using TXS0104EQPWRQ1, but I read a post on this forum that trace length is an issue for the TXS0104EQPWRQ1? The approx. trace lengths are below, I'm not sure how I upload image.
EEPROM > I2C connector for LCD interface (20mm across) > INA228 (25mm across, plus 20mm down on stub > level shifter IC (12mm across) > I2C master (25mm across) > RTC IC (20mm across)
Although this is automotive application, it is not used for anything life critical so we could look at none-automotive part if the feature set is better. Operating temp will be less than 85C. Anti-lock up would be nice.
The LCD I2C controller includes a 10K pull-up, which we have no control over.
Regards
Anders