This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK10034: RX Equalization Settings

Part Number: TLK10034

Hello,

My customer is asking if there are register settings that can be read that provide the RX adaptive equalization settings being applied to the device.

I see that bits 11:8 in register 0x0008 correspond with LS Serdes Equalization control.  Table 5-38 provides the gain settings for the values in this register, however, it only states whether the gain is set to maximum or adaptive, along with some reserve settings.

Are these the only bits available to monitor regarding the RX adaptive equalization settings or is there another register that exposes the settings on which it's locked?

Thanks in advance for your support.

Best Regards,
Brian Gosselin