Part Number: DSLVDS1048
Other Parts Discussed in Thread: DSLVDS1047,
Hello,
I need to convert 100 ohm LVDS signals to 50 ohm single matched LVTTL in both directions. I'd like to use the DSLVDS1048 and DSLVDS1047 dirvers. However, I'm having trouble ensuring that the 50-ohm adaptation will be performed on the LVTTL side. I'd probably have to position a termination resistor on the receiver side and one in series on the transmitter side of the LVTTL. Can these components meet my needs?
Thanks,
Louis