Part Number: DS280DF810
Hello,
I am running unframed PRBS of data-rate 111.81 Gbps from the analyzer over 4 lane @27.9525 Gpbs as shown in the image with serdes loopback at the receiver. We have done the re-timer RX setting to Adaptive Mode 2 for both retimer.
We have the following observation.
1. PRBS is running ok between QSFP-28 to Retimer and from Retimer to QSFP-28
2. PRBS error is detected between ASICS and Retimer
We have the following query
1. Does multiple Retimer in the path can create an issue?
2. Does the CAL_CLK_IN clock have and role in the error?
3. How to calculate and set Pre and post-emphasis to correct the PRBS errors
Regards,
Aman