Part Number: DS280DF810
Hi,

As per the datapath shown above, I am running unframed 103.125Gb/s (100 GE) PRBS on single QSFP port then it is working either it is QSFP 1 or QSFP2 but when I am trying to run PRBS on both the QSFP simultaneously, I am getting BIP-8 error in Port1 lane 2.
To correct the error I tried many possible settings of TX FIR, CTLE and DFE settings of respective retimers but unable to reslove the error.
Please, suggest !!
Also attaching the configuration files of the retimers.
2Port100GE TX settings.cfg2Port100GE RX settings.cfg1Port100GE TX settings.cfg1Port100GE RX settings.cfg