Other Parts Discussed in Thread: THVD1452
Hi Team,
I want to install a node with the RS485 bus line active (hot swapping).
The part to be used is THVD1452DGSR.
What precautions should I take?
Beat Regards,
Teruhito Ishibashi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: THVD1452
Hi Team,
I want to install a node with the RS485 bus line active (hot swapping).
The part to be used is THVD1452DGSR.
What precautions should I take?
Beat Regards,
Teruhito Ishibashi
Hello Ishibashi-san,
So the THVD1452 is hot-swappable. The D, /RE, and DE pins do not have a diode to VCC so max voltage is independent of VCC on the single ended inputs and A , B, Y, and Z are all protected up to +/-15V (recommended) and up to +/-18V (absolute max) independent of VCC.
/RE has a integrated weak pull-up resistor so the receiver stays high-impedance unless you drive the /RE pin low.
DE has an integrated weak pull-down resistor so the driver outputs stay high-z unless you drive DE high.
Y/Z will be high-z as long as DE is low (which it is by default)
A/B is just a receiver pair and will always act as a load regardless - but since /RE by default is high (unless driven low) the corresponding "R" pin output will also be high-z.
So essentially the device when hot-swapped remains hi-z during power up until you actively drive the enables to communicate with the device.
The only real concerns are as follows - and it won't cause damage but it could cause glitches during hot-swap if this isn't followed.
1. Do not have an external pull-up on DE - it could cause the driver to turn on during power up which could cause a glitch - the DE pin has an integrated pull-down.
2. Do not have an external pull-down on /RE - it could cause the receiver to turn on during power up and cause a glitch.
3. Do not short /RE and DE as the default value during hot swap may be be < 2V and cause an indeterminate device state.
Please let me know if you have any other questions and I will see what I can do!
Best,
Parker Dodson