This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75LVCP601: DEx and EQx pins

Part Number: SN75LVCP601

Hi All,

I have a question about the DEx and EQx pins of SN75LVCP601.

The DEx and EQx terminals are connected internally at 2/VCC.
When VCC=3.3V, it becomes 1.65V.
In the case of NC, the DEx and EQx terminals are 1.65V, so wouldn't the DEx and EQx settings be High (=1)?

Best Regards,
Ishiwata