Part Number: DS90UB960-Q1
Hi,
I used the Code Example for Pattern Generator.
It works to CSI0.
When I tried to use the same code to CSI1 it didn't work and I didn't see anything.
What might be the problem?
BR
Shmuel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB960-Q1
Hi,
I used the Code Example for Pattern Generator.
It works to CSI0.
When I tried to use the same code to CSI1 it didn't work and I didn't see anything.
What might be the problem?
BR
Shmuel
Hello Shmuel,
Thank you for your question. Are you selecting CSI1 in the port select register 0x32? This can be done by setting 0x32[1] = 1 prior to the pattern generator code. Additionally, after using the same pattern generation code as CSI0, try setting register 0x21[7] = 1
Regards,
Darrah