Hi,
For ground connected switch with following resistances;
Switch Resistance when open, Rsw_open=50 Kohm
Switch Resistance when closed,Rsw_closed=50 ohm
For 10mA wetting current setting,
Voltage at Inx pin when switch is open= 10mA*50 Kohm=500V.
This exceeds the voltage limit at INx pin which is 40 V maximum.
Can you help with this issue?