Hello TI,
I am using MAX3232 RS-232 transceiver operated at 3.3V. I would like to use either 0.1uF,10%,0201,10V ceramic capacitor or 0.1uF,10%,0402,25V for C1-C4. My question is, the charge pump capacitor voltage can reach upto 6.6V, so is it advisable to use 10V cap due to derating reasons ? If I use 25V capacitor will the capacitance drop since i am operating at 3.3V ? Note : I dont have an option to use 16V capacitor.
Best Regards,
Manoj.