This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8042A: Connect a USB 3.2 hub to a PC with a USB 2.0 port

Part Number: TUSB8042A

Hello,

I would like to use the "TUSB8042A" component to create a USB 3.2 hub. This allows me to expand the number of USB ports on my PC. This hub will connect USB 2.0 devices and USB 3.2 keys.

This hub will be used on different computers (Windows 11, Windows 10 and Windows XP).
If the "TUSB8042A" is connected to a Windows XP computer with a USB 2.0 port, can the "TUSB8042A" work in USB 2.0 or will it be blocked?

I would like the "TUSB8042A" to be a USB 2.0 hub on PCs with USB 2.0 port (Windows XP) and the "TUSB8042A" to be a USB 3.2 hub to PCs with USB 3.2 port (Windows 10 or higher) .

Does this component allow it?

Thank you in advance for your answer.