This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822IF: I would like to inquire about setting DP83822IF fiber??

Part Number: DP83822IF

hi.

Strap set up for DP83822IF fiber drive

After testing, the pull-down straps of RX_D0 and RX_D1 did not work properly

If the pull-down strap of RX_D0, RX_D1 is applied with RH 2.49K pull-up resistance, it is set datasheet  mode 4 

If you check the actual register Set to Mode_1

Is the data sheet wrong?

Datasheet does not say to use pull-up 2.49k for RX_D0 and RX_D1 when using Fiber mode

Please check with the company