Other Parts Discussed in Thread: TUSB1211, TUSB1210
Hi,
I am interested in the TUSB1211 because of its SOF output pin, which would allow me to synchronize several devices to Start Of Frame.
However, the documentation in the datasheet is poor and there is no reference on how to enable this pin. The only thing mentioned is that it needs to be enabled by setting a flag in a specific vendor register but there is no reference made to any register addresses.
Now to my questions:
1. Is there a register description of the TUSB1211 available which would allow me to utilize the SOF output?
2. Is there any timing information of the SOF output, e.g. jitter and delay between USB SOF and the signal appearing on the SOF pin F6 available?
3. What will the SOF pin do in case the TUSB1211 misses one or several Start Of Frames because of transmission errors?
4. If the TUSB1211 is configured to output a 60 MHz ULPI Clock signal on pin A4, is this clock in phase (locked) to the recovered 240 MHz HS-USB clock?
5. What would be the expected jitter on the 60 MHz ULPI clock output?
Any help would be very much appreciated!
Regards,
Fred