This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75LVCP601EVM: CS2298580: SN75LVCP601EVB Board feasibility with Xilinx FPGA board & SATA cable requirements.

Part Number: SN75LVCP601EVM
Other Parts Discussed in Thread: SN75LVCP601,

    We have in-house developed SATA Host IP ported on standard off-the shelf Xilinx FPGA platform. we use GTY transceiver configured for SATA PHY applications. currently we see link errors when we connect the SATA Host with the Analyzer, in order to overcome this issue, we plan to use the SATA re-driver SN75LVCP601 Eval Module between SATA Host & SATA analyzer.

  1.  We are looking to buy "SN75LVCP601 Eval Module", before purchasing we want to check once with the TI Technical Team, can we hook up TI SATA re-driver with SATA Host IP ported on Xilinx FPGA has I/O voltage 1.8 volts. Please comment if any feasibility issues & advice on this? 
  2.  SATA Host FPGA uses FMC to SATA adapter daughter card exposes the SATA 7pin male connector & Viavi SATA analyzer is exposed with SATA 7pin female connector, please suggest SATA cables to be used in order to connect the SN75LVCP601 Eval Module with SATA Host & Analyzer.