Part Number: TCA6416A
Other Parts Discussed in Thread: TCAL6416, TCA8418E, TCA6416
Hi,
We want to use the TCA(L)6416A as an IO Expander of which a many IO's are used as input.
The interrupt output is used to avoid polling, but we can't accept the risk of missing an interrupt when a pending interrupt is cleared during the ACK/NACK of a I2C read cycle, as stated in the datasheet of the TCA6416A, page 9.
Are there options to eliminate this risk without adding additional hardware?
Thanks,
Bert