This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello?
I'm currently considering an RS232 only transceiver. The conditions I'm looking for are as follows.
- Receiver 2-channel, Transmitter 2-channel
- Control Logic Level: 1.8 V
- Power Level: 3.3 V ~ 5 V
- Output Swing Level: Selectable between ±5 V or ±9 V
- Maximum Data Rate: 1 Mbps
- The size of the circuit should be as small as possible
During the review, I saw the only product called THVD4431, but it seems to be large in size with too many channels and features. (40 pins with 5R3T+RS485)
If there is a product other than this that meets these conditions, please recommend it.
Thank you.
S.Y.Lee
Hi S. Y. Lee,
We don't have any device that meets those characteristics listed.
The closest device would be the TRS3122E which has the following parameters:
- 2 Transmitters and 2 Receivers
- Control logic voltage - 1.65V to 5V (through VL pin)
- Main Power Supply - 1.65V to 5V (through VCC pin)
-Output swing voltage - +/-5.4V (typical) when VCC = 3.3V to 5.5V
-Maximum Data-rate: at least 1Mbps @ 500pF loading
-24 pin RGE package - 4mm x 4mm footprint.
The only parameter it doesn't meet is the selectable swing voltage. None of our devices have a selectable swing voltage - and the device that is closest to all your needs is +/-5V (minimum).
Why do need a selectable swing voltage - this is an extremely uncommon need (RS-232 valid voltage levels are +/-5V to +/-15V - so both +/-5 and +/-9V are valid RS-232 voltage levels and would be rated to be placed into the same exact systems). So I am wondering why this is required because I have never seen this as a need in an RS-232 system and the vast majority of RS-232 transceivers, TI or otherwise, also do not give the option of changing swing voltage while also granting a lot of modern features that you are needing. I am just bringing this up because you may be very hard pressed to find a device that meets your system's needs if that is a hard requirement so I'd double check why that is necessary.
Best,
Parker Dodson
To put it briefly, this is an examination of whether it is possible to create a product that can respond at high speeds & low voltage in a weak noise environment and at low speeds & high voltage in a strong noise environment.
Thank you for the detailed review.
I understand that the reason the usable range of RS-232 is ±15 V is for a communication line that is resistant to noise.
So, in my opinion, is it possible to create a product that can respond to ±5.5 V (VCC=3.3V) of 19200~ for short distances (weak noise env.) and ±9.0 V (VCC=5.0V) of 9600 for long distances (strong noise env.).
THVD4421 (currently only EVM is confirmed) seems to match the content except for multi-protocol, but I couldn't find anything other than what I expected, so I asked.
S.Y. Lee
There are RS-232 transceivers that need external high-voltage supplies, e.g., SN75155.
But in practice, high-noise environments are much easier handled with differential signals like LVDS (e.g., SN65LVDS049) or RS-422/RS-485 (e.g., SN65C1168E or 2× THVD1512).
I reviewed the SN75155 you mentioned, but it is not small either. I will also reexamine the overall plan.
Thank you.
Hi S.Y Lee,
As Clemens alluded to - older devices may support multiple supply voltage cases like the SN75155 but they are larger in size and generally have less than ideal performance in many applications.
I will say the THVD4421 - which is only available in the EVM at the moment - is going to have the same issue as our THVD4431 and most of our RS-232 transceivers because you cannot change the swing output voltages for the RS-232 - they are going to be the same as listed in the THVD4431. The THVD4421 is basically the same device as the THVD4431 but with only a 2T2R rs-232 configuration instead of 3T5R. So that won't really work either - the TRS device I listed in my first reply is still the best option that hits almost all of the RS-232 requirements you have.
If you are very concerned about noise I agree with Clemens - RS-485 and RS-422 are most likely better because your speed is only 1Mbps (LVDS is made for very fast communication - like 100s of Mbps - so I don't think that is necessary here). They are differential devices which inherently are more resistant to noise than RS-232 devices are. The two devices Clemens mentioned are okay but they would need a level shifter to be able to use them with a 1.8V controller. However a solution that uses 2x THVD2410V (which is offered in a 3mm x 3mm VSON package - so it is relatively small on the board) would also most likely be a good solution as it allows for a separate 1.8V supply so that it can interface with 1.8V logic - it would include a few other features but ultimately it may be the simplest solution using RS-485. In general if noise is the concern and you have flexibility on what standard can be used I'd highly advise RS-422 or RS-485 - all of our devices that wouldn't require a additional level translator are going to be RS-485 and RS-422 (RS-485 can be thought of as basically a more robust version of RS-422).
Please let me know if you have any other questions and I will see what I can do!
Best,
Parker Dodson