Part Number: DP83826E
1. DP83826E chip, the customer is using RMII mode. The crystal oscillator should be 25MHz or 50MHz?
Besides, for the RMII slave mode, it means the DP83826 is slave, and the MUC ARM is host. Is it right?

2. If the interface does not want to use a transformer, RX/TX only needs to connect a 33nf capacitor in series? Do it still need to pull up to 3.3V or 5V?