This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] FPD-Link Protection

Back to Interface Home Page

FPD-Link Protection

Highlights:

  • FPD Link: Digital audio/video transfer protocol used in video screens or for driver assistance cameras in Automobiles, etc.,
  • Mode of operation: Single ended & differential mode
  • Runs in a 12V line & hence a Protection diode with at least 13.2V breakdown voltage is recommended
  • Max signal transmission speed of up to 4Gbps, requires capacitance less than 1.8pF
  • Automotive applications with localized illumination run on 18V line, requires Vbr ≥ 20.6V & lower capacitance

TI Products Recommendations

Working Voltage (V)

IEC 61000-4-2 ESD Rating (kV) (Contact/Air Gap)

Capacitance (pF)

Channel

count

Package Size (mm)

Package

Recommended for

TPD1E01B04-(Q1)

±3.6

15

0.2

1

1.0 x 0.6

0402

Placement between AC coupling capacitors and the IC

< Related Documentation>

Analog Applications Journal 1Q14

FPD-Link High Speed Design and Channel Requirements

High-Speed Interface Layout Guidelines (Rev. J)

< Related Threads>

Protection Device for DS90UB960

Protection on Serializer Output for DS90UB953-Q1

Can TPD1E0506-Q1 Protect FPD-Link?

Can TPD1E01B04 Protect FPD-Link?

How to Calculate Capacitance Required?

ESD Rating Requirements for FPD-Link

FPD-Link ESD Placement and Requirements