This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] GPIO Protection



Back to Interface Home Page

GPIO Protection

Highlights:

  • Operating Lines: I/Os
  • Dataline operating voltage: 1.8 - 3.3 V, recommended breakdown > 3.6 V
  • Capacitance is not a huge concern < 30 pF
  • Multi-channel recommended for multiple I/Os for space-saving

TI Recommendations

Working Voltage (V)

IEC 61000-4-2 ESD Rating (kV) (Contact/Air Gap)

Capacitance (pF)

Channel

count

Package

ESD351

3.6

30/30

1.8

1

X1SON

TPD4E002

5

15/15

11

4

SOD523

TPD8E003

5.5

12/15

9

8

WSON

< Related Documentation>

ESD Protection for GPIO Pins

< Related Threads>

5V MCU GPIO Protection Options

AM26C31/32 GPIO Protection Options

3.3V GPIO Protection Options

STM32F401VE GPIO Protection Options

5V GPIO High Surge Protection Options