Part Number: THVD1450
Hi team,
Here is the SCH for THVD1450. Could you help to check the SCH and let me know the resistance for R9007?

Thanks,
Leo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Looks OK.
A RS-485 bus should have exactly two termination resistors, at the two ends of the bus.
When the transceiver is at one of the two ends of the bus, the termination resistor should have the same value as the characteristic impedance of the cable; this is typically 120 Ω. When the transceiver is at another place on the bus, then it should not have a termination resistor.