This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB960-Q1: synchronized forwarding mode

Part Number: DS90UB960-Q1

Tool/software:

Hi team,

I follow the sample code in the datasheet to do the FrameSync, it is working well.

But when I streaming output with gsteamer it seems not really same capture frame at the moment.

 here is my pipeline :

gst-launch-1.0 \
v4l2src device=/dev/video-cam0 io-mode=4 ! video/x-raw,width=1280,height=720,format=UYVY ! tiovxldc ! video/x-raw, format=NV12 ! tiovxmultiscaler target=0 ! video/x-raw, width=320, height=240 ! mosaic.sink_0 \
v4l2src device=/dev/video-cam1 io-mode=4 ! video/x-raw,width=1280,height=720,format=UYVY ! tiovxldc ! video/x-raw, format=NV12 ! tiovxmultiscaler target=0 ! video/x-raw, width=320, height=240 ! mosaic.sink_1 \
v4l2src device=/dev/video-cam2 io-mode=4 ! video/x-raw,width=1280,height=720,format=UYVY ! tiovxldc ! video/x-raw, format=NV12 ! tiovxmultiscaler target=0 ! video/x-raw, width=320, height=240 ! mosaic.sink_2 \
v4l2src device=/dev/video-cam3 io-mode=4 ! video/x-raw,width=1280,height=720,format=UYVY ! tiovxldc ! video/x-raw, format=NV12 ! tiovxmultiscaler target=0 ! video/x-raw, width=320, height=240 ! mosaic.sink_3 \
compositor name=mosaic latency=1000000000 background=0 \
sink_0::xpos=0 sink_0::ypos= 0 \
sink_1::xpos=320 sink_1::ypos= 0 \
sink_2::xpos=640 sink_2::ypos= 0 \
sink_3::xpos=959 sink_3::ypos= 0 ! \
video/x-raw, width=1280, height=240 ! queue ! waylandsink sync=false --no-position &

the script for setting FrameSync :

#This sript is for setting 2 ds90ub962 to enable FrameSync mode on ROVY.

DESER_I2C_1=3
DESER_I2C_2=5
UB960_ADDR=0x30
UB960_SR_FS_CTL=0x18
UB960_FS_HIGH_TIME_1=0x19
UB960_FS_HIGH_TIME_0=0x1A
UB960_FS_LOWTIME_1=0x1B
UB960_FS_LOWTIME_0=0x1C
UB960_SR_FPD3_PORT_SEL=0x4C
UB960_SR_GPIO_CTL0=0x6E
UB960_SR_GPIO_CTL1=0x6F
#setting external FrameSync from GPIO1, Generate single FrameSync pulse
FS_MODE_SET=0x98
UB960_SR_GPIO1_PIN_CTL=0x11

#--------------master------------------
    #Enable deserializer#1 GPIO1 and set internal framesync signal
    i2ctransfer -y -f $DESER_I2C_1 w2@$UB960_ADDR $UB960_SR_GPIO1_PIN_CTL 0x91
    #Set FS_HIGH_TIME_1
    i2ctransfer -y -f $DESER_I2C_1 w2@$UB960_ADDR $UB960_FS_HIGH_TIME_1 0x0A
    #Set FS_HIGH_TIME_0
    i2ctransfer -y -f $DESER_I2C_1 w2@$UB960_ADDR $UB960_FS_HIGH_TIME_0 0xD7
    #Set FS_LOWTIME_1
    i2ctransfer -y -f $DESER_I2C_1 w2@$UB960_ADDR $UB960_FS_LOWTIME_1 0x61
    #Set FS_LOWTIME_0
    i2ctransfer -y -f $DESER_I2C_1 w2@$UB960_ADDR $UB960_FS_LOWTIME_0 0xA0
    #Enable framesync
    i2ctransfer -y -f $DESER_I2C_1 w2@$UB960_ADDR $UB960_SR_FS_CTL 0x01
    
#--------------slave-------------------
    #Setting FrameSync mode
    i2ctransfer -y -f $DESER_I2C_2 w2@$UB960_ADDR $UB960_SR_FS_CTL $FS_MODE_SET

#--------------gpio-------------------
    #Setting deserializer #1 & #2 back channel GPIO0,1,2,3 output FrameSync
    for RX_NUM in {0..3}; do
        RX_PORT=$(((1<<$RX_NUM)+($RX_NUM<<4)))

        i2ctransfer -y -f $DESER_I2C_1 w2@$UB960_ADDR $UB960_SR_FPD3_PORT_SEL $RX_PORT
        i2ctransfer -y -f $DESER_I2C_1 w2@$UB960_ADDR $UB960_SR_GPIO_CTL0 0xAA
        i2ctransfer -y -f $DESER_I2C_1 w2@$UB960_ADDR $UB960_SR_GPIO_CTL1 0xAA

        i2ctransfer -y -f $DESER_I2C_2 w2@$UB960_ADDR $UB960_SR_FPD3_PORT_SEL $RX_PORT
        i2ctransfer -y -f $DESER_I2C_2 w2@$UB960_ADDR $UB960_SR_GPIO_CTL0 0xAA
        i2ctransfer -y -f $DESER_I2C_2 w2@$UB960_ADDR $UB960_SR_GPIO_CTL1 0xAA
    done

I'm not sure is it causing by what, so I want make 4 camera can output synchronized .

the script for setting synchronized forwarding :

DESER_I2C_1=3
DESER_I2C_2=5
UB960_SR_FWD_CTL1=0x20
UB960_SR_FWD_CTL2=0x21

#--------------fwd sync mode-------------------
#all RX port forwarding enabled 
    i2ctransfer -y -f $DESER_I2C_1 w2@$UB960_ADDR $UB960_SR_FWD_CTL1 0x00
    i2ctransfer -y -f $DESER_I2C_2 w2@$UB960_ADDR $UB960_SR_FWD_CTL1 0x00
    sleep 0.1
#basic synchronized forwarding enabled
    i2ctransfer -y -f $DESER_I2C_1 w2@$UB960_ADDR $UB960_SR_FWD_CTL2 0x14
    i2ctransfer -y -f $DESER_I2C_2 w2@$UB960_ADDR $UB960_SR_FWD_CTL2 0x14

The display streaming will stuck after run the script.

here is the ds90ub960 i2c dump :

root@rovy-4vm:/opt/edgeai-gst-apps# i2cdump -y -f 5 0x30
No size specified (using byte-data access)
     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f    0123456789abcdef
00: 60 00 1e 40 d0 01 00 fe 1c 10 7a 7a 00 09 00 ff    `.?@??.???zz.?..
10: 00 00 00 00 00 00 00 00 90 00 00 00 00 00 04 00    ........?.....?.
20: 00 14 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ??..............
30: 00 00 01 40 00 00 00 00 00 00 00 00 00 00 00 00    ..?@............
40: 00 a9 71 01 00 00 20 00 00 00 00 12 38 c0 02 00    .?q?.. ....?8??.
50: 00 00 00 00 00 00 00 00 1e 00 00 00 00 00 00 00    ........?.......
60: 00 00 00 00 00 00 00 00 00 00 00 00 00 7c aa aa    .............|??
70: eb ec e4 00 00 00 00 c5 00 01 00 00 20 00 00 00    ???....?.?.. ...
80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
90: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
a0: 00 00 00 00 00 1c 00 00 00 00 00 00 00 00 00 00    .....?..........
b0: 1c 3a 14 08 25 00 18 00 8c 33 83 74 80 00 00 00    ?:??%.?.?3?t?...
c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
d0: 00 43 94 05 60 f2 00 00 00 00 00 00 00 00 00 00    .C??`?..........
e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
f0: 5f 55 42 39 36 30 00 00 00 00 00 00 00 00 00 00    _UB960..........

I did some experiments and found it seems related to some port be enable the forwarding.

For example once I turned port 2 and 3 off, the streaming was start to run. but looks not really good, the display delay over 2 seconds and framerate less than 10 fps. (original 30fps)

 i2ctransfer -y -f 5 w2@0x30 0x20 0xc0 //enable forwarding of port0 ,1 
 

The problem does not occur in any specific port, even I change enable port 2 & 3, disable any one port or enable 1 port. 

But those issue doesn't happened when setting the synchronized forwarding disabled, all the camera are work good, no latency and 30 fps smoothly. 

So I think my camera signal source are good, did I miss any configuration ?