Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869
Tool/software:
Hi,
We've integrated the DP83869HM with our Linux system and are attempting to use it with a Fibre connection. We've added it to the device tree and added the dp83869 driver to our Kernel build. It appears the PHY is discovered by the Kernel but the link is not up. We've looked through the PHY registers and confirmed everything is in the correct mode. Disconnecting and reconnecting the fiber connection does not display any messages.
Using ifconfig, we can configure an IP and ping the connection, as long as it's on the local network. However, we have a second PHY on the board connected to copper and it seems that the communication is being routed through this one. Pinging of the PHY connected to fiber does not work if the copper is disconnected.
We've had a look through the troubleshooting guide but haven't found anything to help us with this issue.
Thanks,
Rory