This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCA9515A: PCA9515APWT & PCA9515APWR

Part Number: PCA9515A
Other Parts Discussed in Thread: TCA9517A, TCA9617B

Tool/software:

What is the difference between T & R in following part PCA9515APWT & PCA9515APWR.

Datasheet is not available for PCA9515APWT

is this package difference? If yes, please share evidence doc

Please clarify

  • Hi Shan,

    The 4th is a holiday. Please give a day for feedback, thanks. 

    Best Regards,

    Michael. 

  • Hi Shan,

    I believe the difference lies in the packaging. Since the PCA9515APWT is discontinued, I am not sure on the specifics, but if I had to guess, one is tape and reel packaging, and the other is just tape without the reel. 

    Datasheet is not available because this specific device was discontinued, but the PCA9515A datasheet should still be the same and accessible. 

    PW - TSSOP should have same package dimensions between the two devices, just different manufacturing package options either tape and reel or just tape. 

    Also, I would suggest moving away from the PCA9515A. This device is older technology and contains a device errata with clock stretching. This issue has been common among different customers, with the only fix of replacing the part. Devices such as TCA9517A or TCA9617B do not have this problem, and are made with new process technology, I also expect the supply of this device to be more long term. 

    Regards,

    Tyler