Part Number: TCAN4550
Tool/software:
Hi team, my customer used TCAN4550 in their project, could you help to review the SCH design?

BR
Jingguo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN4550
Tool/software:
Hi team, my customer used TCAN4550 in their project, could you help to review the SCH design?

BR
Jingguo
Hi Jingguo,
I have reviewed the schematic and I have the following comments:
- The nWKRQ pin should not be connected to GND because this will be driven to a 3.6V voltage during Sleep Mode and this will result in a large current flow with a direct connection to GND. If this pin is going to be unused in the system, it should be left unconnected.
- The RST pin is "Active High" and should be held "LOW" for normal operation. The RST pin is also being pulled to +3.3V instead of the +5V-CAN rail being supplied to VIO and for all of the other digital IO signals. I don't know if this is an intentional decision.
- The VSUP supply voltage needs to be greater than 6V due to the internal 5V LDO. Using the +5V-CAN voltage will be too low and the device will be held in an under-voltage protected mode. The VSUP should be connected to the +12V supply rail.
- The SPI Chip Select pin (nCS) must be connected to the processor with the rest of the SPI signals. It must transition from High-to-Low at the beginning of the SPI read/write transaction, remain Low for the duration of the data, and then transition from Low-to-High at the end of the transaction. If the nCS signal does not transition, then SPI communication will not work. Please refer to the SPI programming section of the datasheet.
- The Interrupt pin (nINT) is an open-drain architecture that requires a pull-up resistor to the VIO supply rail.
- It is recommended to include a series resistor between the OSC1 pin and the crystal to help optimize the circuit for stable performance. A 0-ohm resistor can be used and adjusted to a different value later if needed. Please see the TCAN455x Clock Optimization and Design Guidelines Application Note (Link)
- The crystal load capacitors are connected to a different GND than the rest of the device.
Regards,
Jonathan