Part Number: TLK10081
Other Parts Discussed in Thread: DP83869HM
Tool/software:
Hello,
I'm currently using a TLK10081 with 7 lanes (4 Ethernet lanes and 3 SFP lanes) as it follow :

My problem is that I have asymmetrical performances by passing through the TLK10081 when performing a speedtest
With the TLK10081 :
Speedtest results :Download ~ 800Mbps Upload ~ 50Mbps with packet loss
Direct connection as reference, without TLK10081
Speedtest results : Download ~ 800Mbps Upload ~ 800Mbps without packet loss (direct transmission between two DP83869HM is ok with symmetrical performances).
TLK10081 config I use :
read 0x02
read 0x06
write 0x00 0x8610
wait 1sec
write 0x01 0x0302
write 0x02 0x831B
write 0x06 0x8114
write 0x8009 0xFC02
write 0x8019 0xFC02
write 0x1C 0x002C
write 0x1D 0x002C
write 0x17 0x0ABC
read 0x02
read 0x06
wait 5sec
write 0x17 0x02BC
Do you have any recommandation or anything that I can change in the config to solve this issue ?
Thank you in advance.