This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
First:DS160PT801 I/O power is 1.8V。when i used usb2any connect to DS160PT801, Is the I2C interface of USB2ANY 3.3V or 1.8V?
Second: used DS160PT801 for PCIE X8 ( 8LAN FOR TX,8LAN FOR RX)。 can i use usb2any config DS160PT801 and write EEPROM?
Third: Can you provide a firmware HEX file for PCIE X8? So I can burn it into EEPROM first