Tool/software:
Hi at TI, I have a 947 to 928 communication issue.
I can talk via i2c from the 947 to a screen with the 928.
I can reach the remote devices in the screen no problem(microcontroller and touch controller)
I can read local registers(0x5A) that tell me the link is in the single TX mode as expected so not problem.
All this time there is no Oldi input to the 947.
As soon as I turn the video on(Dual Oldi) to the 947.
For and instant I can see from 0x5A that the link is ready, TX active and RX locked, still single TX on port0, and Oldi flags good.
Then next read of that register shows link not ready, and back to dual TX mode, the default setting.
Anyone got any thoughts on this - plainly I am doing something wrong.
Thanks in advance for any suggestions
William