Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UA9637A: RS485/RS422 differential input with

Part Number: UA9637A
Other Parts Discussed in Thread: THVD2410

Tool/software:

Hi.

I am looking for a input differential receiver that has integrated fault detection (open circuit, short-circuit) 

  • Hi Andres,

    All THVDXXXX devices have open, short, and idle bus failsafe built-in. The THVD2410 specifically has the highest range of fault protection up to +/-70V on the bus. However these are standard 1 transmitter, 1 receiver devices.

    If 2 receivers are still required, you can use a 2 THVD1400s as receivers only for example. All THVDXXXX devices are complaint with both RS-485 and RS-422 standards. We currently do not have differential receivers with open and short circuit protection. 

    Best, 

    Ethan

  • Andres,

    I realized that I might have misunderstood your question. Are you seeking a device that merely protects against short circuit condition (my assumption), or are you seeking a device that has separate output pin that flags when there is a fault on the bus? All of the devices I mentioned above do not explicitly flag if there is a fault.

    Regards,

    Ethan

  • A device that has separate output pins that flags when there is a fault on the bus

  • Andres,

    At this time, we do not have a device that flags an output when there is a fault on the bus. 

    Regards,

    Ethan

  • Most faults result in both lines being pulled together through the termination resistors, which results in a differential bus voltage of 0 V. This can be detected by connecting two receivers with exchanged A/B pins; when both output high, the bus is in an invalid state.

    When you do not have external fail-safe resistors, this triggers also when the bus is idle.