Part Number: DS90UB941AS-Q1
Other Parts Discussed in Thread: ALP
Tool/software:
Background: Occasional flash screen issues with LT7911+TI941 projects.
1. The software for debugging large-screen projects only changes the EDID resolution from 1920X720->800X480.
Small screen display fixed flash screen, the same firmware can be displayed normally when the LT7911D development board is connected to other DSI receiving.
Part of TI941 is abnormal
Suspected pairing problems with TI941;
(Compared with the normal display on the large screen, TI needs to explain whether the DSI->TI941->TI948 and DSI->TI941->TI926 signal paths have different requirements for DSI (DSI CLK/DSI DATA))
2. The LT7911D DSI output is configured in non-homologous mode
The repeated flash screen measurement confirms that DSI CLK in non-homologous mode is around 81MHz.
In homologous mode, DSI CLK frequency is about 83MHz,
TI needs to confirm that DSI CLK is around 81MHz.
TI941 collects why the screen flashes,
If pixclk is restored based on the DSI clock,
DSI clock bias affects recovery pixclk frequency resulting in different frame rates,
But should not cause the screen fixed flash screen;
3. TI926 output HS difference and internal recovery synchronization signal logic require TI support.
4. In addition, TI948 output LVDS also has HS/VS, whether the HS/VS logic is the same