Other Parts Discussed in Thread: TUSB1210, TUSB1211
When using the TUSB1210 in a Host Application where the connecting client does not need VBUS, only DP and DM communcations, can the VBUS and ID pins on the TUSB1210 IC remain NCs?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
John,
ID pin is used to determine of the TUSB1210 is in host or peripheral mode. In OTG applications, this is handled by the cable. For permanent host applications, then ID must be grounded.
The VBUS pin of the TUSB1210 is not needed in stand-alone host mode. However, your system is required per the USB spec to be a power supplier on the VBUS line.
dear sir, in our design (based on OMAP3630 + TUSB1210), the only usb device, an on-board wcdma modem module, is separately powered and needs only D+/D- communication with TUSB1210. According to your answer, my understanding is that we can leave VBUS and CPEN pins floating, is that correct?
Tianfu Ma
I'm also wondering how to handle TUSB1210 VBUS pin in this situation. A 10K pullup to 5V rail gives a VBUS pin voltage of ~2.2V. What exactly is the VBUS pin doing, and how should it be terminated if not connected to a supply? (we float CPEN, ID is grounded, this is a special embedded controller application.)
thanks . . . lasher
Hi Jeffrey,
Please find VBUS connection recommendations and background information below which I hope will answer your question.
Best regards,
Peter CONSIDINE
(TUSB1210, TUSB1211 design lead)
ANSWER:
- TUSB121x does not strictly require VBUS to function.
- If VBUS detection is not required by the link then:
- If VBUS detection is required by the link but VBUS pin is not connected to TUSB121x then:
- Note that connecting VBUS to VBAT pin is not recommended as VBAT cannot be guaranteed to be > VA_VBUS_VLD comparator level (4.65Vmin).