Other Parts Discussed in Thread: TS12A12511
Is there such a thing as RS232 buffer and RS232 multiplexer?
RS232 is different from normal interface as it gives a -3 to -25V for logic low and +3 to +25V for logic high vs normal interface which gives a 0 for logic low and +5V for logic high.
Hence selecting a buffer for RS232 requires the buffer to be able to take in -25V to +25V and output accordingly.
I would like the buffer to be a fanout, meaning 1 RS232 input to the buffer will generate 2 RS232 output with same voltage level as input.
Similarly, a multiplexer for RS232 would need to take such voltage.
Could recommend such chip if possible.