I want to design an LVDS to TTL interface board for small LCD’s (4.3 – 5.7”) range. I am having trouble finding an IC to handle this. TI Flatlink SN65LVDS308 is close but it only has 2 serial receivers, voltage is 1.8 but a level shifter could handle that. I don’t think 2 chips would be an option due to the clock pair impedance supplying both chips. Would you be able to recommend another option to achieve this translation?
Specs:
LCD clock: 5 – 30MHz
Voltage level: 3.3V
LVDS input Channels: 4
Parallel outputs: 27
Thanks,
Adam