This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
reverse MII is the name for a reverse loop of data. you might either refer to the MII loopback which loops back data received on the MII tx data (data which originated at the MAC) to the MII rx data. or you might have referred to the far end reverse loopback which enables the PHY to loopback DATA received on the RJ45 RX pair to the RJ45 (RJ45 is connected to the line, the copper wire medium) TX pair. you can find more information on TLK110 data sheet on chapter 3.10 Loopback functionality. http://www.ti.com/product/tlk110
Thanks,
Aviad
Hi Hithesh,
you can read more material on all the loopbacks available on the TLK110 device in the data sheet http://www.ti.com/product/tlk110 chapter 3.10 Loopback functionality.
Thanks,
Aviad
Hey,
it also refers to direct MAC to MAC connections, meaning that no PHY is involved.
For instance, look here: http://www.eetimes.com/document.asp?doc_id=1275925.
Brgds,
Giorgos