Part Number: DP83849I
Other Parts Discussed in Thread: DP83826E, DP83822I, DP83825I
Hello. I'm looking for a TI product that can solve my problem. I have a ASIC chip which has a Ethernet MAC MII interface (10/100 speed) and it needs to talk to a CPU which also has a MAC MII interface & USB2 interface. I've read that you can't connect MAC MII to MAC MII directly - the protocol won't work. Is that true? Basically I need an expert on Ethernet IEEE 802.3.
Otherwise I need some sort of 'bridge' chip to connect the two together. What has TI got?
I think there are two possible solutions:-
1) Use a 2-port ETH Switch chip and connect the PHY's together. Therefore ASIC MAC MII to ETH SW MAC MII, short both PHY outputs together, then ETH SW MAC MII to CPU MAC MII.
2) Use a USB2 to PHY bridge. Though I can't find one that outputs a MAC MII interface. I presume I have to connect it to another single port ETH PHY/MII chip (i.e. similar to option 1 above).
Note: ASIC VIO is 1.8V