I posted this question into industrial interface forum,
and later, I found Ethernet forum. so, I posted it again.
===================================================================================
I have one question about dp83849I. (Actually it may be general questions about MDI trace routing.)
According to design and layout guidelines, MDI signal traces should have 50 ohm to ground or 100 ohm differenctial impedance.
If I use 4 layer, 2T, 1oz PCB, in case of microstrip, the trace width should be more than 0.6mm to meet 50/100 ohm impedance. but your pin width is just max 0.27. How can I meet the impedance requirement?
Even in your DEMO board reference design (snlc021), your MDI trace( on the top layer ) width seems to be just less than 0.27.
If I used stripped line scheme, I should make some vias, but also, your design guideline recommend not to use via.
I am a little bit confused. I am very novice for ethernet.
please let me get more insights on this subject.
Thank you for your advice in advance.
Best Regards
Hak-Jin Jeong