Other Parts Discussed in Thread: TUSB8040A1, TUSB7340
I am analysing TUSB8040A1 USB 3.0 Four Port Hub and TUSB7340-SuperSpeed USB 4�Port xHCI Host Controller for connecting it to my microcontroller providing maximum data at256Mbps. As per there specifications both can support upto 4 devices/hub and connects to PC.
DO we need any specific software on the pc for the host controller to run it?
Do we need any specific USB3.0 device controller as the other end of the hub or can we connect directly with microcontroller via SPI bus or GPIO ports etc? Can they be linked as host-hub-device?
Even if the hubs are powered, cant i connect 50 microcontrollers in a daisy chain.