This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Please let me know whether the following points for SN65HVD01 IBIS model are correct.
Regarding the definition of [Ramp], AB_hs's [Ramp] are smaller than AB_ls's. Is this correct ?
※AB_hs high speed AB buffer operation
[Ramp]
R_load = 27
dV/dt_r 1.31081/5.41776e-09(typ) 0.971551/1.10314e-08(min) 1.57638/3.70288e-09(max)
dV/dt_f 1.18121/5.49901e-09(typ) 0.973025/9.69578e-09(min) 1.36243/3.64603e-09(max)
※AB_ls low speed AB buffer operation
[Ramp]
R_load = 27
dV/dt_r 1.31059/4.98207e-09(typ) 0.971543/1.04064e-08(min) 1.57601/3.41618e-09(max)
dV/dt_f 1.09683/5.29281e-09(typ) 0.854744/9.37254e-09(min) 1.32391/3.5372e-09(max)
Best Regards,
Kato
Max - san,
Thank you for the reply. Customers think this is a problem. So, would you change the revision for the new model ?
Best Regards,
Kato