Other Parts Discussed in Thread: TUSB9261
My customer is designing in the TUSB9261 on his Sitara board. The SATA interface connects to a compact flash (CFast) from Cactus Technologies, which supports S.M.A.R.T., a feature the customer wishes to utilize.
The customer has the TUSB9261 EVM and has it connected to his Sitara board which is running Linux kernel v3.2.0. Cactus' code uses SCSI ATA Translation (SAT) to access the SMART data from the flash device. The customer is using SAT as well, but his code hangs whenever an attempt to access the SMART information from the flash card is made.
I have found other E2E posts which indicate (or imply) the TUSB9261 supports SAT (SCSI ATA Translation), but nothing stating definitively that SMART diagnostics are covered.
Can you confirm SMART support for the 9261 or give any advice to help move this along? Thanks in advance.