This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I need to convert a 1.2V differential signal from a Xilinx FPGA to a 3.3V HDMI TMDS signal. It must also be able to achieve data rates above 3.4Gb/s per TMDS pair for my application. Will the TMDS181 work for my application. What is a HDMI retimer? What is a HDMI redriver?
Hi William,
100nF caps are required in AC coupled lines; regarding size and materials we use 0402 and 0201 mostly ceramic capacitors.
Regards
Hi Moises,
I am having difficulty understanding what I need to do with the control pins. It says in the datasheet linked below for the SNx5DP159 that the pin strap mode is available to configure the device if I2C is not available under section 9.2.1. Does this mean that if I2C is available I should not use the pin strap mode and set the I2C_EN/PIN to high for I2C control mode? What is pin strapping I have not heard the terminology before? Is there any advantage to using I2C over pin strapping?
Hi William,
Pin strapping mode is juts GPIO mode to configure the device.
It dependce on what you want to do if GPIO or I²C is the configuration method you need.
using I²C gives you acces yo a wide range of configurations, using GPIO you can configure a few options.
It depends on your applications what you need to use GPIO or I²C.
Regards
Hi Moises,
Thank you for your explanation I now understand that pin strapping is just pulling the control pins high or low or leaving them floating. So if I enable the I2C bus by pulling the I2C_EN/PIN pin high can I leave the other control pins (16,17,23 & 34) in figure 30 floating as the pin strapping mode will be disabled?
Hi Moises,
I would like to ask you in figure 30 and 31 (www.ti.com/.../sn65dp159.pdf) why are there no 50 ohm termination resistors? But there are 50 ohm termination resistors in figure 4 of the following application note (www.ti.com/.../slla358.pdf).
Best regards,
William.
Hi Moises,
Thanks for clarifying that I would also like to know why does the HDMI case have a 1M ohm resistor and 10nF capacitor in parallel attached to the HDMI receptacle? In figures 31 and 32 of the datasheet http://www.ti.com/lit/ds/symlink/sn65dp159.pdf
Best regards,
William.
Hi Moises,
I have not been able to find the voltage rating of the capacitor connected to the chassis in the HDMI specification, what do you recommend?
Best regards,
William.
Hi,
I can see that there are 4x 100nF capacitors that would be presumably be placed as close as possible to the pads 12, (19,20), 31 and 40. But what do I do with the 2x 10nF capacitors? I was under the impression that smaller value caps had to be placed the closest to the pads? Which pads do I need to place them near and why isn't there 4x 10nF capacitors or 1 10nF capacitor per pad (with the exception of 19,20 as they are adjacent)?