This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hola Luis,
You mentioned that the latency for TX data path is 933-973 (4 lanes) = 93.3-97.3ns (full rate 10Gbps).
Meanwhile for RX data path is 475-515UI (4 lanes) = 47.5-51.5ns (full rate 10Gbps), these values includes
the data path from Low speed side to High Speed side.
Basically, we want to implement transponder application and it will operate at 2.4576G、3.072G、6.144G and 9.8304G.
We will use TLK10002 or TLK10232 as new project design. If the TLK10031 can be half price of TLK10232 and we will choose TLK10031.
Below figure is our application...so, our high speed will have 4 different line speeds.
BTW I need to know that does the UI for latency calculation will change follow by the line rate?
That means:1/9.8304、1/6.144、1/3.072、1/2.4576ns. Or, will it have different formula to calculate?
I will use 1:4 mode only and 153.6MHz reference clock.
Hi Jacky,
1. Yes, even this configuration is the recommendation in datasheet for TLK devices.
2. Basically the TLK10232 is the new generation of the TLK10002, although the TLK10232 has another features such as:
Supports 10GBASE-KR, XAUI and 1GBASE-KX.
Attached you will find a quick comparison between both devices.
Best Regards,
Luis Omar Moran
High Speed Interface
SWAT Team
Hola Luis,
Great answer and thank you very so much.
BTW, I have two final questions below:
1. CPRI --> HS TLK10232 LS --> LS TLK10232 HS --> CPRI?right?
2. "Does 2.4576G” will be?
1084 / 2.4576 = 441ns
1522 / 2.4576 = 619ns
So, the total delay will be (441 + 619) x 2 = 2120ns for 2 chips?
Brs
Hello Jacky,
Please let me know if you have further questions.
Regards,
Luis