Other Parts Discussed in Thread: TRS3221, SN74AUP1T50
Hi,
I am using the TRS3221 in a UART application (PC -> DB9 -> TRS3221). The logic level for my device is 2.5V (3.3V input tolerant) therefore I am using a level shifter, SN74AUP1T50, only on DIN.
My question is, do I need a pull up on DIN?
Secondly, I noticed that the TRS3221 inverts the input before putting it on the output. Is that typical UART operation?
Thanks.