Other Parts Discussed in Thread: DS110RT410
Hello,
My customer is considering DS110RT410 for 10Gpbs Ethernet.
He has questions about DS110RT410.
[Q1]
Do you have a sample configuration examples of recommended register settings for 10 Gigabit Ethernet?
(About the address of register and the recommended setting that need for 10 Gigabit Ethernet )
[Q2]
The description of the address 0x64 of DS110RT410 data sheet (page 47), have been described as
"Must also program channel register 0x67[7]" and "Must also program channel register 0x67[6]".
However, the register 0x67 are reserved.
Is this the correct?
My custermer set bits 7:6 of register 0x67 to value of 2'b11.
But, value 2'b00 are readed from bits 7:6 of register 0x67.
Data sheet has been described as "RW".
Can this register (0x67) write and read?
Best regards,
Hiroaki Masumoto