Other Parts Discussed in Thread: SN65HVD233-Q1
Dear, Sir.
My custommer try to use SN65HVD233-Q1 as CAN PHY. Unfortunately, CAN Bus application
is first time for them, so they are requesting the recommended schematic & component for it.
I founf the user's guide, SLLU234.
I would like to make sure as below. Please help us.
1. All component value is not defined on the guide.
It is possible to clarify that?
2. R11/R12 Termination.
I wonder these terminations are needed to connect active system CAN Bus?
3. TXD & RXD.
I wonder the series resistors, pull-up resistors & capacitors are needed?
4. Choke coil & TVS.
Is it possible to clarify recommended part number or spec?
Best Regards,
H. Sakai