Part Number: DS80PCI800
Other Parts Discussed in Thread: DS80PCI810, , DS125BR111, DS100BR111
Tool/software: WEBENCH® Design Tools
Dear Sir
Do you have the user guide to teach how to use this tool ??
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS80PCI800
Other Parts Discussed in Thread: DS80PCI810, , DS125BR111, DS100BR111
Tool/software: WEBENCH® Design Tools
Dear Sir
Do you have the user guide to teach how to use this tool ??
Thanks
Hi Kai,
It is not a user guide, but this presentation does go over some WEBENCH simulations in a PCIe application.
Hopefully this can get you started.
PCI Simulations with WEBENCH Interface Designer.pdf
Best Regards,
Lee
Hi Kai,
Since you have moved to the most sensitive Signal Detect threshold and there are still errors, the only thing still open to try is forcing the DS80PCI800 output to remain active. The 20" of trace and 2 cables must represent a significant level of signal loss.
To force the outputs to stay active SMBus access is required.
The following DS80PCI800 registers must be written
Reg Value
0x06 = 18'h
0x0D = 02'h
0x14 = 02'h
0x1B = 02'h
0x22 = 02'h
0x2A = 02'h
0x31 = 02'h
0x38 = 02'h
0x3F = 02'h
Regards,
Lee
Kai,
The numbers are from various sources and simulations. The circuits are very similar and respond in the same way. There is only one table for both devices.
The change in numbers likely comes from the low frequency used to calculate the high frequency gain.
Regards,
Lee