Part Number: TPS65982
Hi,
I have programmed and verified my new TPS65982 device (custom board) using both the Snapshot and Aardvark Flash Center GUIs. When I download the programming from Flash center I am able to see the contents written on the flash memory (using the same memory that came with the eval board). Here is a screenshot of my program download:
The issue is that I am stuck in BOOT mode and never move into APP mode:
Boot flags are also showing as bad:
Boot Flags (0x2d)
Re-read Register Clear Status
Status: Register Read SUCCESS
BootOk False
ExtPhvSwitch False
DeadBatteryFlag False
SpiFlashPresent True
Region0 True
Region1 True
Region0Invalid True
Region1Invalid True
Region0FlashErr False
Region1FlashErr False
UartCRCFail False
Region0CRCFail False
Region1CRCFail False
CustomerOTPInvalid False
OneCallI2COtpBits 0x1
App Cust Version Error False
App Cust Length Error True
App Cust CRC Error False
Debug Ctl 1 state at boot low
Debug Ctl 2 state at boot low
DevNumber 0
UartBoot False
UartOverflowErr False
IntPhvSwitch False
UartRetryErr False
UartTimeoutErr False
OTPValid 2
SWD Disable False
Vout3v3Ctl True
WaitForVin3V3 False
OneCallI2cOtpBits 1
Vout3v3Threshold 6
REV_ID_Metal 0
REV_ID_Base 0
Could you please guide me on how to troubleshoot this issue?