This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2543: TPS2543 Configuration

Part Number: TPS2543
Other Parts Discussed in Thread: TMS320F28069

Hi,

Application: (Single USB Port on a Embedded System)

1. User will Use to Charge Mobile (5V @ 1Amps) from this Embedded System.

2. Developer will use to store data in Pen drive from this Embedded System .

Below is the Schematic:

Doubts:

1. Is CDP Mode Choosen, correct for this application.

2. Hardwiring Ctrl 1, Ctrl 2, Ctrl 3, I_Lim_select Pins is Correct  (?) (Pin 6,7,8,4)

3. As Enable Pin is also hardwired, Can status and fault pins left unconnected?

Regards,

Siddharth Gupta