Other Parts Discussed in Thread: TPS65981
It is probably me and I am missing the information but I want to know about maximum power dissipation from this device, I was planning to follow the example layout exactly from the datasheet but this doesn't state whether the layout is good for the entire current range (20V/5A or what kind of thermal performance I would get if I followed that layout.
I would be using a thin 4-8 layer board, really I want to know what kind of losses I am going to expect with this device and how much heat it is going to produce at max
Also does anyone have any information on when the TPS5990 datasheet is going to completed? I would like to use it in a product but the datasheet is not completed
Best wishes
Sam