Hi Sir/Mdm,
The Vcc spec is narrower at 5V +/- 0.5% and what is the impact if the Vcc supply voltage drop to range 4.5V to 4.75V?
Regard's
Jason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir/Mdm,
The Vcc spec is narrower at 5V +/- 0.5% and what is the impact if the Vcc supply voltage drop to range 4.5V to 4.75V?
Regard's
Jason
Jason,
The SN65LBC176A needs a minimum Vcc of 4.75V and maximum of 5.25V which is a tolerance of +/- 5%. We cannot guarantee that this device will function with Vcc less than 4.75. We have newer devices that can handle lower Vcc if that would be better for your application.
Respectfully,
Lucas Schulte