Part Number: ISO5852S
To whom it may concern,
The ISO5852S IC is used to drive the SiC MOSFETs (1200V/523A) in the ongoing project we are currently working on. We are also using the desat detection option of the mentioned IC, unfortunatelly the soft turn-off function doesn't seem to work. In the attached .pdf file, I am providing the schematic of the gate driver circuit, together with the measurements obtained during the fault condition.
The nominal DC voltage that we have in the system is 800V. But, as you can see on the waveforms, due to non-existent soft turn-off the drain-to-source voltage shoots up to 750V with approximately 400V at the input.
Can you comment on why the soft turn-off function is not working? We are not using the inverting BJT pair on the output of the gate driver, since it is stated in the data sheet of the device that it is not compatible with desat logic.
Best regards,
Milos Stojadinovic